Part Number: SN6501
Other Parts Discussed in Thread: SN6505B
I have a product design with SN6501 transformer driver. I used the reference design specified in the datasheet, from 3V3 to 5V, with 750313769 transformer.
I use the converter with load current in 5 to 10 mA range.
If I compare my measurement results with the efficiency specification in the datasheet (Figure 20), my efficiency is much lower. The datasheet specifies an efficiency between 70 and 80%, but I measure an efficiency between 55 and 70% (i.e. more than 10% lower).
See attached document for more details.
Does someone know where this big difference comes from?