This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1432: SIN COS Encoder Signals

Part Number: ISO1432
Other Parts Discussed in Thread: UA9638, ISO7720,

My customer would like to use ISO1432 to replace the ISO7720+UA9638 and TLP2366(Opto Coupler) on Motor Encoder application. Please find here for configurations between CNC controller and Servo Drive. 

Is there any side effect? Or any advice? 

  • Hi Brian,

    Thank you for posting to E2E!

    Is our customer looking to operate the servo drives using RS-485? Can you share a part number for the Servo Drives?

    Using ISO1432 may require additional hardware changes. Please allow me to confirm this alternative is suitable with the larger team and provide a response on Monday or Tuesday next week during business hours.


    Best,
    Manuel Chavez

  • In general, the ISO1432 can serve as a replacement for multi-chip isolated RS 422 solutions such as the ISO7720+UA9638. The details of this thread are being handled via email.

    Respectfully,

    Lucas