This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Thanks for reaching out.
Yes, ISO1410 is pin-to-pin compatible with ADM2483BRWZ with just one difference on Pin7 which is PV for ADM2483 and is NC for ISO1410. Device ADM2843 requires the PV pin to be driven by LOW during power-up to avoid some chatter on A/B pins. While ISO1410 doesn't have any such restriction and there is no such need for PV pin to maintain chatter free data transmission on A/B. Hence, this is not connected internally to device and named NC (Not Connected).
Hence, replacing ADM2483 with ISO1410 should be just fine. Even if customer application has some PV logic implemented, applying such a signal to ISO1410 doesn't affect the device and will continue work without any issues.
Please see below a few more advantages of ISO1410 over ADM2483.
Regards,
Koteshwar Rao
Hi Team,
thanks for your great support.
BTW another question , How about MAX2202X ?
Has TI solution P2P with MAX2202X ? or similar soluiton
Thanks!
Hi Jimmy,
Sorry, I missed to address your question on MAX2202x.
We do not have a P2P device for MAX2202x family but ISO1410 should meet most of MAX2202x specs, though in a different package. We also have ISO1500 which is an RS-485 isolator in a smaller package, maybe this is of interest to customer. Please do check if either of these devices can be used. Thanks.
Regards,
Koteshwar Rao