This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was wondering if it's possible,using the TPS7B7702-Q1, to short the LIMx pins to GND and tie the OUTx pins together in order to achieve a higher output current closer to 500mA (550mA is the internal limit)?
Cheers,
Joe Howard
Hello Jason,
I'm wondering if it would be possible to share current between the two outputs of the TPS7B7702 to allow for one single output at 500mA. We have an app note on LDO current sharing using ballast resistors:
Given the tolerance of the device regulation, my calculations led me to pretty sizable resistors (around 3 ohms) in series with the outputs, which would certainly cause a large voltage drop at the output at 500mA.
Another scheme I saw utilized a current sensing mechanism to control the feedback of one of the outputs in order to balance currents without the need for ballast resistors: '
In this case, a difference amplifier was implemented with the current input (or output) being sensed at both LDOs. Would it be possible to implement a scheme like this by utilizing the built-in current sensing feature of the TPS7B7702?
Thanks,
Casey