This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Appro IPNC & G711 Audio Encoding : Problem with Streaming in RTSP



Hello,

I am for my debug using the IPNC version 1.0 of the code. We are in the course of ordering the version 2.5 of the DM365 IPNC.

My problem is : we are recording audio samples from an external codec and we have checked that the pcm samples are OK when recorded on the platform (so the driver layer is OK). We input a sinus signal at 1KHz or 100Hz for a sampling at 8000Hz on 1 channel.

When listening at VLC we hear that the sound signal is not continuous. Image is smooth.

My question is : is there some network / streaming properties problems which have found in the subsequent release of IPNC (from version 1.0) which showed this problem of audio samples discontinuous ?

Because now, debugging the Appro Interface in relation to the network application wis-streamer will not be so "easy".

Thank you for your answer.

reda

  • An information I found when printing debug messages in stream.c : I printed the timestamps of the audio frames when put on the shared memory and they are all separated by 256 ms. When each frame is considered to be 125ms long, and since we are in mono, it is strange to see this gap. Do not know yet if this gap results in the discontinuous audio signal heard in VLC. What I can see anyway is that the network RTP data payload are separated by the same amount of around 250ms. So the problem may come principally from the av_server and not wis-streamer ?

    Any clue ? Is that a known bug on the version 1.0 ?

  • Hi,

     

    Version 1.0 is more than a year and half old release. can you please migrate to latest release avaialble at Appro ftp site and check if this issues exists?

     

    Regards,

     

    Raghu

     

  •  

    Hello Raghu,

    We are in the course of migration (ordering version 2.5 from Appro is in the pipe). I wanted to be sure that the problem was identified on the 1.0 version and had been fixed on subsequent versions, and especially the 2.5 we are ordering.

    Thanks for your info about this topic.

  • HI, version 2.6 should be uploaded this week. Please use this as this will be the latest.

     

    Regards,

     

    Raghu

     

  • Hi Raghu,

    my TI sales representative told me that for DM365 there won't be any more version above the 2.5. Are you sure the version 2.6 is for this device or is it for DM368 ?

    Thanks

     

  • Version 2.6 is for DM365 as well as for DM368, it is a common release.

    This should be uploaded at Appro ftp site by this week

     

    Regards,

     

    Raghu

     

  • Version 2.6 for DM368, is fixed ?
    I test H264 1080P & G.711 Audio in version 2.6, but video is not smooth and audio is not continues.

  • Hi,

     

    Can you please give more details on the issue you are facing, please share the logs and recoded avi files with audio/video

    one more check, have you updated the UBL, uboot from the v2.6?

     

    Regards,

     

    Raghu

     

  • I am updated the UBL and U-Boot to v2.6.

    But that has bad block table found message in boot time.

     

    I test configures as follow,

    H264, D1 Audio OK

          720P/1080P Audio not continues

     

    MPEG4, D1/720P Audio OK

           1080P Audio not continues

     

    ----------------------------------------

    DM36x initialization passed!

    TI UBL Base Version: 1.50

    Boot Loader BootMode = NAND

    Starting NAND Copy...

    Valid magicnum, 0xA1ACED66, found in block 0x00000008.

    Boot Mode Task Completed

     

    IPNC UBL Version: 1.1.0

    Platform: DM368

     

    Jumping to entry point at 0x81080000

     

    U-Boot 1.3.4 (Dec  9 2010 - 17:44:14) DM368-IPNC-1.0.1

     

    I2C:   ready

    DRAM:  128 MB

    NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,               3V 8-bit)

    Bad block table found at page 65472, version 0x01

    Bad block table found at page 65408, version 0x01

    128 MiB

    In:    serial

    Out:   serial

    Err:   serial

    ARM Clock :- 432MHz

    DDR Clock :- 340MHz

    Ethernet PHY: GENERIC @ 0x01

    Hit any key to stop autoboot:  0

    DM368 IPNC :>

    -------------------------------------------

     

     

  • Hello,

    I encounter the same strange behaviour. Is the problem fixed in IPNC26 or is there at least some information available how to solve the issue?

    Kind regards,

    Marc Jüttner

  • Hi,

    Can you please explain the problem you are observing?

    PLease share the log and issue details.

    Regards,

    Raghu

  • Raghu,

    thanks for the quick response! We face the same issue as mentioned above. Based on IPNC15 with most changes from IPNC2.6, we ported the entire software suite to DVSDK4 and notice strange timestamps when streaming audio (which is interrupted in an irregular interval between one and two seconds on the RTSP client-side). The logs show this:

    ---

    <snip>

    AUDIO: Create...
    Audio Sample File opened
    AUDIO_GetSampleRate - CurrentStatus is = 8000
    AUDIO : period size = 1000 frames dir = 0
    AUDIO : period time = 125000 us dir = 0
    Plug PCM: Hardware PCM card 0 'DaVinci DM36x' device 0 subdevice 0
    Its setup is:
      stream       : CAPTURE
      access       : RW_INTERLEAVED
      format       : S16_LE
      subformat    : STD
      channels     : 1
      rate         : 8000
      exact rate   : 8000 (8000/1)
      msbits       : 16
      buffer_size  : 16000
      period_size  : 1000
      period_time  : 125000
      tstamp_mode  : NONE
      period_step  : 1
      avail_min    : 1000
      period_event : 0
      start_threshold  : 1
      stop_threshold   : 16000
      silence_threshold: 0
      silence_size : 0
      boundary     : 2097152000
      appl_ptr     : 0
      hw_ptr       : 0

     AUDIO: Create...DONE
     AUDIO: Start...
     AUDIO: Start...DONE

    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684505365)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684505366)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684505613)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684505614)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684505862)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684505863)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684506111)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684506112)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684506360)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684506361)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684506610)]
    AUDIO_audioTskRun - AudioBufInfo ready [(1000, 684506611)]
    <snip>
    ---

    As one can see, the timestamps are not at all correct. Regarding the sampling rate, we expect the timestamps to increase by 125ms for each sample block, but we see them increase by ~250ms in the first read and by 0-1 ms in the second read, and so on. Shouldn't they be equidistant?

    Our anaylsis turns out that the streaming server comes out of sync due to the malformed timestamps.

    So my question is: Is the issue fixed in IPNC2.6, e.g. did we forget something in our porting work? Any hints or explanations?

    Thanks in advance,

    Marc Jüttner