Hello,
I am for my debug using the IPNC version 1.0 of the code. We are in the course of ordering the version 2.5 of the DM365 IPNC.
My problem is : we are recording audio samples from an external codec and we have checked that the pcm samples are OK when recorded on the platform (so the driver layer is OK). We input a sinus signal at 1KHz or 100Hz for a sampling at 8000Hz on 1 channel.
When listening at VLC we hear that the sound signal is not continuous. Image is smooth.
My question is : is there some network / streaming properties problems which have found in the subsequent release of IPNC (from version 1.0) which showed this problem of audio samples discontinuous ?
Because now, debugging the Appro Interface in relation to the network application wis-streamer will not be so "easy".
Thank you for your answer.
reda