Other Parts Discussed in Thread: TIDA-00002, ADS1278-HT, TMS470R1B1M, SM470R1B1M-HT, REF5025-HT
Hi,
I got a HEATEVM REV B board ( that is,TIDA-00002 ) and I need to use it for down hole drilling. I have few questions about using it.
1. As the User Guide says, we need external power. now I have a power supply board which can convert 12V to 3.3V,1.8V and 5V. Do I just link the power line to JP2, or I should generate the power-up sequence of ADS1278-HT and SM470R1B1M by myself ? Has "the Power HEATEVM" been released?
2. Does HEATEVM GUI Software (Rev. A) also work for TIDA-00002? If does, In order to run this application,what should I do on the board,which jumpers should be jumpered?
3.I want to use the IAR embeded workbench for ARM to develop it. I build the example from example project for TMS470R1B1M, and use J-Link to download the bin file, but it can not connect the target. Does anybody know how to use the IAR to develop for TIDA-00002? Maybe I should solve the power problem first.
Regards,
Shaw