This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In an electronic board we are using the AM26LV31E-EP differential line driver.
For the LIGHTNING qualification test, we need to inject a burst of voltage pulses (in both polarities) into the individual outputs of the AM26LV31E-EP (protected with TVS).
The datasheet shown the Vo (Output voltage range) ABSOLUTE MAXIMUM RATINGS (–0.5V / 6V).
What does this parameter represent? Is it the maximum voltage that I can force at the output?
What is the maximum continuous voltage I can force in the driver outputs?
What is the maximum voltage pulse that the driver outputs can withstand (amplitude, duration, duty cycle)?
Thanks and best regards.
Thank you very much.
We should withstand the LIGHTNING test as per RTCA/DO-160F Section 22 Category A3XXX.
Each AM26LV31E-EP output is connected to a unidirectional Transient Voltage Suppression diode( TVS) with a clamping voltage of +5V.
Therefore each output will have to withstand (one pin at a time) a burst of pulses of about +7V/130us and -900mV/130us. The time between each single stroke is about 2s.
The stoke generator will be connected with 5Ohm resistor in series.
Do you think we can withstand the LIGHTNING test?
In this regard I found a discussion in the TI E2 Community:
https://e2e.ti.com/support/interface/industrial_interface/f/142/t/111592
but it is not clear to me if the TVS used are able to protect the AM26LV31E-EP outputs.
Thank you very much.