This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There seems to be an ongoing discrepancy with the reference voltage specified for this part, or we have been supplied with a very old part.
A colleague calculated the feedback resistors for a 3.0V output using this device, ironically using an old data sheet dated May 2001, the reference voltage he used was 1.224V, he calculated R1 at 348k and R2 at 240k, measured voltage 2.98V which is correct. When I checked his calculations, I used the datasheet from your website which is dated December 2009, page 8 specifies the feedback voltage as 1.127V, using this and the resistor values given above the output should measure 2.76V, it does not. The part fitted has the marking PCFI, does this indicate is we have been supplied old stock? My concern is that in the future we will receive new stock and the resistor values will then be wrong.
Any guidance is appreciated.