Part Number: TXB0102
Other Parts Discussed in Thread: SN74AXC2T245
TXB0102 for UART Application
TXB0102 is used for UART translation usually. Will following scenario cause some problem?
- Power on the target board first, VCCA and VCCB are supplied.
- Then connect UART cable to the target board.
What we worry about is that, UART RXD could be Hi-Z for both sides. (One side is input and the other side is floating.)
Perhaps, TXB0102 is configured in wrong direction, since both sides are Hi-Z. Will it make any trouble when we connect UART cable at this moment?
Thanks,
- Charles Lai