Part Number: SN74HCS00
Other Parts Discussed in Thread: SN74LVC74A, SN74LVC1G74
I noticed all 74HCS gates and some other functions all have a Cpd of 10pF in your datasheets.
Now in other families like 74HC or 74LVC , their Cpd's vary a lot depending on which gate.
How come for HCS this is a "clean" 10 pF (for all) ? Preliminary numbers ?? Really ? A year after their introduction?
How can I compare a 74HCS00 to a 74AHC132 (11pF) if the uniform 10pF of HCS is not trustworthy?
Follow up questions :
From your datasheets: LVC00 Cpd :19pF , LVC02 9,5pF , LVC32 12,5pF and LVC10 11pF .
I tested them in the 5 Mhz to 31Mhz range: The LVC00 's 19pF is is about right , LVC02's 9,5pF is no way ,
it draws just above the LVC00 . LVC32's 12,5pF consumes even more , LVC10's 11pF , again more than
the LVC00 and between the LVC02 and LVC32.
So the LVC's 19pF is about right but the other 3 consume more , much more than their wrong Cpd numbers suggest .
How do you calculate these Cpd numbers because they are wrong . Errors on the datasheets ? No one notices
after decades since they have been available?
If a gate has 2 inputs , are the Cpd values when using the 2 inputs together or just on 1 with the other not blocking
the gate , like on the Vcc for a NAND gate ?
74LVC74 has Cpd 26pF but its little logic brother 74LVC1G74 has Cpd of 37 (both at 3,3V) !
How is this possible? Many more inconsistencies in Cpd throughout your datasheets of Cmos logic.