Part Number: SN74AXC4T774
Hi LVT Team,
I have a customer using the SN74AXC4T774, and I wanted to make sure that we were understanding the drive capabilities of the device correctly.
The driving capabilities seemed to be outlined in Section 6.15 of the datasheet with the source and sink charts.
Are the source and sync capabilities of the output independent of the VCC on the input? So for example if they wanted to translate from 1.2 to 3.3V the VCCB in question would be 3.3V and would be the same regardless of VCCA. Am I understanding this correct?
Thanks,
Mitchell