Part Number: SN74ACT244
Other Parts Discussed in Thread: DAC80508
Hi Team,
I would like to generate a sine signal that swings between 0V and +5V.
The frequency is around 6.8KHz. Can I generate such a signal keeping the nOE pin low and providing PWM at the input pins.
My controller providing the PWM is a 3.3 V logic.
Also, If I need to bypass the SN74ACT244 with another signal generator like DAC or something, do I need to break the connection at the output or just change the state of the nOE pin to logic high?.
My doubt is does the buffer will have any effect on my system if I bypass the SN74ACT244 keeping the nOE pin high. Or do I need to connect the output of the SN74ACT244 to my system through a zero-ohm resistor and remove the resistor when bypassing the SN74ACT244?.