This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT1G04: Is it Possiable to use a Inverting buffer/driver like SN74AHCT1G04 with 5V Power supply, 3.3V Sinewave input, to generate a inverted 5V Sinewave in Output Y ?

Part Number: SN74AHCT1G04


Dear

when using an active crystal oscillator to output an 3.3V Sinewave, we want to change the 3.3V Sinewave to 5V sinewave.

Is it OK to use a  Inverting buffer/driver like SN74AHCT1G04 with 5V Power supply, 3.3V Sinewave input, to generate a inverted 5V Sinewave in Output Y ?

When powered with 5V, the output waveform is 5V? or 3.3V ?

Thanks!