This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC1G14: pspice for TI : missing parameter in TI supplied model for sn74ahc1g14

Part Number: SN74AHC1G14


parameter 'maxICC' appears to be missing. this is the same error as one a few weeks ago for another AHC series part. Please provide an updated library model for this part. its not clear if the parameter should be the same as the part  reported a few weeks ago. thank you

pspice for TI missing parameter.pdf

**** INCLUDING SCHEMATIC1.net ****
* source TRANSISTOR_DIGITAL
V_V2 N16654 0 3.3Vdc
C_C1 0 N16654 10p TC=0,0
V_V3 N17681 0
+SIN 1.65 1.65 40e6 0 0 0
C_C2 N17681 N17139 1n TC=0,0
R_R1 N17139 N16654 10k TC=0,0
R_R2 0 N17139 10k TC=0,0
X_U6 N16654 N17139 N16654 0 SN74AHC1G14

**** RESUMING bias.cir ****
.END
+ V(BETA,3#)*V(CURR_OUT,3#)}
X_U6.XU1.XUA.EREF X_U6.XU1.XUA.NREF 0 VALUE {0.5*(1 - V(BETA,3#))*(V(VTRP_P,
+ 3#) + V(VTRP_N,3#))+ 0.5*V(BETA,3#)*(V(NTRUE,3#) + V(NFALSE,3#))}
X_U6.XU1.XUA.EDIFF X_U6.XU1.XUA.NDIFF 0 VALUE {V(NFB,NREF)}
X_U6.XU1.XUA.ESWITCH X_U6.XU1.XUA.VSWITCH 0 VALUE {0.5*(-SGN(V(NDIFF,3#))
+ + ABS(SGN(V(NDIFF,3#))))}
X_U6.XU1.XUA.ESWITCH1 X_U6.XU1.XUA.VSWITCH1 0 VALUE {0.5*(SGN(V(NDIFF,3#))
+ + ABS(SGN(V(NDIFF,3#))))}
X_U6.XU1.XUA.GCOMP 0 X_U6.XU1.XUA.CURR_OUT VALUE {SCHMITT_TRIGGER_INPUT_SELECT*0.5*V(
+ 2#,3#)*(SGN(V(NDIFF,3#)) + ABS(SGN(V(NDIFF,3#))))}
X_U6.XU1.XUA.GSTD 0 X_U6.XU1.XUA.CURR_OUT VALUE {STANDARD_INPUT_SELECT*0.5*V(
+ 2#,3#)*(SGN(V(1#,VSTD_THR))+ ABS(SGN(V(1#,VSTD_THR))))}
X_U6.XU1.XUA.ROUT X_U6.XU1.XUA.CURR_OUT 0 1
X_U6.XU1.XUA.EMID X_U6.XU1.XUA.MID 0 VALUE {0.5*(V(2#,3#) + V(3#))}
X_U6.XU1.XUA.EARG X_U6.XU1.XUA.NARG 0 VALUE {V(CURR_OUT,3#) - V(MID,3#)}
X_U6.XU1.XUA.EOUT X_U6.XU1.NA 0 VALUE {0.5*(SGN(V(NARG,3#)) + ABS(SGN(V(
+ NARG,3#) ) ) )}
.PARAM MAXICC maxICC
--------------$
ERROR(ORPSIM-16152): Invalid number: Error while converting token 'maxICC' to double value. Token can be a constant or expression
+ V(BETA,3#)*V(CURR_OUT,3#)}
X_U6.XU1.XUB.EREF X_U6.XU1.XUB.NREF 0 VALUE {0.5*(1 - V(BETA,3#))*(V(VTRP_P,
+ 3#) + V(VTRP_N,3#))+ 0.5*V(BETA,3#)*(V(NTRUE,3#) + V(NFALSE,3#))}
X_U6.XU1.XUB.EDIFF X_U6.XU1.XUB.NDIFF 0 VALUE {V(NFB,NREF)}
X_U6.XU1.XUB.ESWITCH X_U6.XU1.XUB.VSWITCH 0 VALUE {0.5*(-SGN(V(NDIFF,3#))
+ + ABS(SGN(V(NDIFF,3#))))}
X_U6.XU1.XUB.ESWITCH1 X_U6.XU1.XUB.VSWITCH1 0 VALUE {0.5*(SGN(V(NDIFF,3#))
+ + ABS(SGN(V(NDIFF,3#))))}
X_U6.XU1.XUB.GCOMP 0 X_U6.XU1.XUB.CURR_OUT VALUE {SCHMITT_TRIGGER_INPUT_SELECT*0.5*V(
+ 2#,3#)*(SGN(V(NDIFF,3#)) + ABS(SGN(V(NDIFF,3#))))}
X_U6.XU1.XUB.GSTD 0 X_U6.XU1.XUB.CURR_OUT VALUE {STANDARD_INPUT_SELECT*0.5*V(
+ 2#,3#)*(SGN(V(1#,VSTD_THR))+ ABS(SGN(V(1#,VSTD_THR))))}
X_U6.XU1.XUB.ROUT X_U6.XU1.XUB.CURR_OUT 0 1
X_U6.XU1.XUB.EMID X_U6.XU1.XUB.MID 0 VALUE {0.5*(V(2#,3#) + V(3#))}
X_U6.XU1.XUB.EARG X_U6.XU1.XUB.NARG 0 VALUE {V(CURR_OUT,3#) - V(MID,3#)}
X_U6.XU1.XUB.EOUT X_U6.XU1.NB 0 VALUE {0.5*(SGN(V(NARG,3#)) + ABS(SGN(V(
+ NARG,3#) ) ) )}
.PARAM MAXICC maxICC
--------------$
ERROR(ORPSIM-16152): Invalid number: Error while converting token 'maxICC' to double value. Token can be a constant or expression