Part Number: SN74LV165A
Other Parts Discussed in Thread: SN74HCS165
The schematic See link https://note.youdao.com/s/abxHhbAr ,VCC is DC5V. the parameter Δt/ΔV,for VCC=4.5V to 5.5V,the max is 20ns/V. Does it mean the max is 70ns from 0V to 3.5V. The CLK wave CLKrise1-80ns(0-5V)、CLKrise2-120ns(0-5V),please see link https://note.youdao.com/s/MwlbY7Rh. Do they meet the requirements?
How much capacitance value on the CLK pin of SN74LV165A?
thank you!