Part Number: SN74LVCC4245A
Hello,
Were are investigating a board returned for logic failure.
We would like to know if an overcurrent protection exists on the component 74LVCC4245.
We did tests on our board equipped with the component.
Configuration: VCCA = 5V VCCB = 3.3V
Direction set from B to A
3.3V applied on B2 so A2 is driven high to 5V
Test: We applied a short circuit on A2 output.
Results :
The VCCA still around 5V
Io on A2 was measured at 300mA few seconds before a continuous 290mA.
Vo on A2 was measured around 155mV Test: 3.3V applied on B2 so A2 is driven high to 5V
Results :
Vo on A2 was measured around 5V. OK
Visual inspection: No dammage on the component.
What do you think about this behaviour ?