Part Number: TXS02612
We are currently considering a circuit using TXS02612 to connect Xilinx XC7Z030 -1 FFG 676 I from the MicroSD card slot.
I referred to the circuit diagram of zedboard of xilinx, but there are some parts I don't understand, so I asked you.
The questions are as follows.
1.Do I need to pull up the CMDB0 signal?
If necessary, please tell me the reason for pull-up.
2.Is resistance required between CLKA and FPGA?
How do you determine this resistance value?
3.Is there a recommended resistance for the SEL PD?
4.Is there a recommended circuit for TXS02612?
zedboard schematic for reference
reference.digilentinc.com/.../zed_sch_rev_f1-public.pdf
6p of the above schematic
Thank you very much.