Can down translation work from port A to port B? I have my circuit configured in such a way (5 -> 3.3). From supplemental material, such as the YouTube video, it seems clear that this is not the recommended means of down conversion. However, I didn't gather that from the datasheet and treated the device as any other translator. Without pull-up resistors, logic highs on the B side are 2.4 volts instead of the desired 3.3 volts. Is there a way to salvage what I have with the correct pull-ups for a prototype unit? Or should I simply start over with the proper configuration?