Other Parts Discussed in Thread: SN74LVC1G34, SN74LV1T125
Hello,
I am currently using the SN74LV1T34 (DCK package) to shift a 3.3V PWM signal of a few MHz to a 4.096 level signal. This is then just low pass filter averaged and passed into an output driver, so there is negligible current draw from the SN74LV1T34. This works perfectly as implemented.
We are having availability issues with the SN74LV1T34, so I am looking for a replacement. I currently have pin 1 of the SN74LV1T34 tied to ground, so I was also looking at the SN74LV1T125, however this is unavailable as well. I was hoping the SN74LVC1G34 would work here. It doesn't specifically specify up translation, but looking at the datasheet and my application I'm not seeing a reason why it wouldn't work. The input PWM signal will always hit the high and low voltage levels.
Am I correct in thinking the SN74LVC1G34 will work in this application? Is there another replacement that could work? The logic needs to not be inverted, and at this point, I am locked into the DCK package.
Thank you!