Part Number: SN74HC14
Other Parts Discussed in Thread: UCC27517, SN74LVC1G14
Hi Team
When using Schmitt triggers to control MOS , but the output current does not reach the current required for MOS conduct (e.g. Schmitt triggers single channel maximum output 25mA, but actual MOS on-current may be up to 200mA) Would this portion of the power supply damage the Schmitt trigger?
It's just about moment that instance 200 mA, probably within 100 ns, is needed to charge the capacitor to turn on MOS, is this continuous 25mA enough to charge the capacitor to turn on the MOS , it may cause a delay to turn on. But Will this damage the schmitt trigger?

Best Regards