Hello Team,
the datasheet for the SN74AXC4T774, as other devices without the schmitt trigger input, points out that the input should never float.
There is also the application note describing the reason. This is ok and understood.
Not being floating, brings also a minimum rise time for any voltage change. To avoid being in the "unknown" state area for long period.
- If I have only 10pF load, what could be the pull up resistors I can use to avoid having floating input and not create problem for the rise/fall time ? (datasheet has Input transition rise or fall rate being max 5ns/V
- Is it the pull up value a realistic pull-up?
Thanks,
SunSet