Hi
I found the USB to SPI bridge solution, but the SPI voltage level of the USB-SPI bridge is 3.3V, so I need the level-shift (1.8V-3.3V) component. I chose the "SN74AXC4T774BQB", would you help check if the SN74AXC4T774BQB is workable?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I found the USB to SPI bridge solution, but the SPI voltage level of the USB-SPI bridge is 3.3V, so I need the level-shift (1.8V-3.3V) component. I chose the "SN74AXC4T774BQB", would you help check if the SN74AXC4T774BQB is workable?
Thanks.
Hi
I have another question about the signal data rate. In the datasheet description, The translated signal data rate can be up to 310 Mbps when the signal is translated from 1.8V to 3.3V. but I would like to know if the translated signal data rate can also be up to 310 Mbps when the signal is translated from 3.3V to 1.8V? Thanks
Derek.
Yes, the SN74AXC4T774 can translate SPI signals at these voltages.
As shown in sections 6.11 and 6.13 of the datasheet, the maximum propagation delay for 1.8 V to 3.3 V is 7 ns, while for 3.3 V to 1.8 V, it is 5 ns or 6 ns. So you should be able to get the same speed. What frequency do you need?
Hey Derek,
This device should have no issue with that frequency and is a great fit for the SPI directionality.