Hi,
I have a question regarding the unused input on SN74LVCH32373A. Looks like the recommendation in section 7.1 and 8.2.1.2 are contradictory, could you advise.
Thanks,
SB
In section 7.1 Overview:
Active bus-hold circuitry holds unused or undriven inputs at a valid logic state. Use of pull-up or pull-down
resistors with the bus-hold circuitry is not recommended.
8.2.1.2 Input Considerations
Unused inputs must be terminated to either VCC or ground. These can be directly terminated if the input is
completely unused, or they can be connected with a pull-up or pull-down resistor if the input is to be used
sometimes, but not always. A pull-up resistor is used for a default state of HIGH, and a pull-down resistor is used
for a default state of LOW.