This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC16T245: SN74AVC16T245

Part Number: SN74AVC16T245
Other Parts Discussed in Thread: SN74AUC244

Hello

SN74AVC16T245 an support 80MHz clock signal. From B -> To A

VCCA=1.8V

VCCB=2.5V

Thanks

Roi

  • Hey Roi,

    We don't spec data rate for this part so I can't say for sure, but 80 Mhz may be hard to achieve with the output supply of 1.8 V. If you are only down translating, I would recommend using two SN74AUC244 devices supplied with 1.8 V. It has overvoltage tolerant inputs that will accept the 2.5 V and should achieve that speed with little issue.