Other Parts Discussed in Thread: SN74LXC8T245, SN74AHC367, SN74AHCT367, SN74AHC541, SN74AHCT541
Hi
I used TXB0106 as UART level shifter
V_CCA as 3.3V, V_CCB as 5V
The problem is the higher peak of translated level(3.3 to 5) shows well and low side also until I connect something(just test by oscillator), after connect other sensors or sth, low side can't reach to 0V that makes the logic hesitates to recognize low level while high level goes well.
I tried to apply a pulldown resistors(0, 51K, 1M) but no effect
I used STM32F4VE (3.3V based logic) board to make signal
since STM board should already had capacitors, I first had no other bypasses
I directly connected V_CCA to OE
thanks