This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC1G08: (SN74AHC1G08DBVR)Design check

Part Number: SN74AHC1G08

Hi There,

               If the input pin(pin1/pin2) goes hi earlier than VCC pin, will the leakage occurs on VCC(pin5) / output pin (pin4) / the other input pin(pin2/pin1)?

  • Hello,

    The input voltage on A or B can be up to 5.5V, independent of the supply voltage.

    Leakage current is always going to flow from higher voltage to lower voltage pins. The maximum leakage current for the device is defined here: