This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G11: Input and output current limit

Part Number: SN74LVC1G11


HI Team,

I am using SN74LVC1G11DBVR.

1.Input current limit per pin (A.B.C pins) is 5uA?

2. If the logic high input that I am driving is in mA, should I limit this current using a series resistor?

But IIK limit is 50mA. 

3. Can this gate output be connected as a logic input to another gate?

Please clarify.

Thanks,

Vidhya