Hi,
I am using TXB0108.
Some I/O ports are unused.
The processing of an unused terminal is pull-up or pull-down.
Here, I have the question.
What is recommended value of resistor?
For instance,I think as follows.
PULL-UP.
MIN value:VCCx÷50mA.(note:x is A or B.)
Because it doesn't exceed absolute maximum rating IO(50mA).
MAX value:4kohm.
Because the unused terminal input voltage is sure to become VCCI/2 or more.
Is this correct?
Correct me if I am wrong.
Thanks for reading!
Toshiya.