Part Number: LSF0108
Hi,
We are using a level converter (LSF0108PWR) to convert 3.3V (Vref B) to 1.8V (Verf A) able to measure the channel A signals logic voltages are 1.8V. But in Channel B signal logic voltages is 2.1 instead of 3.3V for B6, B7, B8 signals and the rest of the B1, B2, B3, B4, B5 channel signal logic voltage is 1.8V instead of 3.3V.
And When I connected EN (low) to GND, The channel B signal logic voltages are 3.3V for B6, B7, B8 signals and the rest of the B1, B2, B3, B4, B5 channel signal logic voltage is 0V instead of 3.3V.
Please verify the below schematic and suggest if any changes are required.


Regards,
Gajendiran A