This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: High level input is not confirmed

Part Number: TXB0108
Other Parts Discussed in Thread: TXS0108E

For unavoidable reasons, FETs are used for level conversion of external 24V equipment, connected to TXB0108 and input to FPGA.

I have the following connections

FPGA(3.3V) <- A:TXB0108:B <- (5V 10kΩPU)Drain:FET:Gate <- 24Vsystem Device with  voltage device resistor

The 24V device was connected, and it was confirmed that the drain voltage of the FET alone was HI: 5V and LOW: 0V.

When TXB0108 is connected to the drain of the FET, the HI level potential becomes about 2V, and HI level detection does not work well.

How can I determine the HI level?