Part Number: TXS0104E
Hello,
Are there any precautions for the TXS0104 output driver? Is there a restriction that the capacitive load is up to 70pf like the TXB series?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXS0104E
Hello,
Are there any precautions for the TXS0104 output driver? Is there a restriction that the capacitive load is up to 70pf like the TXB series?
The TXS has edge accelerators which drive high for a short time (like the TXB). If the capacitive load is larger than 70 pF, the output voltage might not reach VCC immediately.
But the TXS has integrated pull-up resistors, so the output voltage will rise eventually. This might or might not be fast enough for you.
Thanks,
Please tell me about the following. I'm assuming it will be used with low speed interface like I2C (400KHz).
Their capacitive load is greater than 70pF depending on the trace length and cable.
Is there any problem?
>But the TXS has integrated pull-up resistors, so the output voltage will rise eventually. This might or might not be fast enough for you.
It's fast enough for I²C. The edge accelerators would be needed to reach 2000 kHz.
I understand that TXS is fast enough for I²C and UART.
But, Do we have to consider that the capacitive load exceeds 70pF ?
TXS has a pull-up resistor, so don't worry about it?