This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AC14: Problem in Altium Pspice simulation

Part Number: SN74AC14


Hello,

for my simulation I downloaded the SN74AC14 Spice model and used it by Altium.

It has a strange behavior as you can see by the attached images; it seems that the input impedance on the A input is 0.01 ohm, as you can see the current in R4 is 330A (V1 is generating a pulse of amplitude 3.3V.

I noticed that because I tried to put two inverter in series and the output of the second one is always zero.

Could someone help me? Is there something I am doing wrong?

Thanks

Domenico