Hi Team,
Customer request Tc,Tj,Ta,θjc,θjb,θja ,Ψjt,Ψjb,Ψja for SN74HC595PWR.
Could you help provide that?
Thank you!
Marc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Marc,
The maximum junction temperature is in the datasheet: 150°C
Ambient temperature is in the datasheet: -40°C to +85°C
Case temperature is not provided.
Other values for the PW package, all in °C/W:
Result- Theta JA-High K (standard datasheet value) | 103.5 |
Result-Theta JC, top (standard datasheet value) | 38.5 |
Result-Theta JB (standard datasheet value) | 48.5 |
Result- Psi JT (standard datasheet value) | 3.3 |
Result- Psi JB (standard datasheet value) | 47.9 |