Other Parts Discussed in Thread: SN74ALVTH162827
Hello,
What isolation level does SN74LVT244B support, Level 0, Level 1, Level 2 or Level 3?
Any compatible devices working at 1.8V power supply?
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What isolation level does SN74LVT244B support, Level 0, Level 1, Level 2 or Level 3?
Any compatible devices working at 1.8V power supply?
Best regards,
K.Hirano
Hello Hirano-san,
I believe the isolation level you are referring to comes from the application report Logic in Live-Insertion Applications With a Focus on GTLP
In this application report the levels are defined as:
Level 0 - normal device
Level 1 - Partial power down
Level 2 - Hot insertion
Level 3 - Live insertion
-
For Level 1, a device must include the partial power down feature and specification (Ioff)
For Level 2, a device must include Level 1, the Power-Up 3-State (PU3S) feature and speicfication (Δt/ΔVCC Power-up ramp rate)
For Level 3, a device must include Level 2, the precharged I/O feature and specification (VBIAS pin)
-
Hopefully this has already answered your question, but to be clear, the SN74LT244B includes both Ioff and Power-Up 3-State support, but not Bias VCC, so it is a Level 2 device.
Additionally, it says "Hot Insertion" on the front page, which is the name of the Level 2 isolation.

Emrys,
Thank you for your response.
Let me confirm one more thing.
TI does not have a similar device working at 1.8V, right?
Best regards,
K.Hirano
Hello Hirano-san,
The lowest voltage device with the PU3S feature is the SN74ALVTH162827, which can operate down to 2.3V. I don't know of any that can reach 1.8V.
This is the search I used: https://www.ti.com/logic-voltage-translation/buffers-drivers-transceivers/noninverting/products.html#p2192=Power%20up%203-state&p1498=Catalog&sort=p0min;asc