SN74AXCH8T245PWR is out of stock, and replace it with SN74LVH8T245PWR. The maximum working temperature of SN74AXCH8T245PWR is 125℃, but the maximum working temperature is 85℃. The board temperature of customer is 90℃. If over temperature, what is the risk of SN74LVH8T245PWR--this 8bit dual-supply bus transceiver?