Part Number: TXS0102
Other Parts Discussed in Thread: SN74AXC2T245, SN74LVC2G66
Can the TXS0102 drive a 2nF capacitive load when operating push-pull as a UART level shifter? 115.2kbps, 3.3V on both sides.
Also, is it okay if VCCA is slightly higher than VCCB (say 0.1V higher) if our 3.3V regulators on both sides are not set exactly the same?
Thank you,
Ben