Other Parts Discussed in Thread: LSF0101, SN74AXC1T45
Hi,
can two TXB0101 be connected in series or what would be a suitable solution to connect a 1V8 system bidirectionally to the input of a 3V3 TXB0101?

Thanks and regards,
Manuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
can two TXB0101 be connected in series or what would be a suitable solution to connect a 1V8 system bidirectionally to the input of a 3V3 TXB0101?

Thanks and regards,
Manuel
No. TXB inputs require other devices to have a drive strength of at least 2 mA (see section 9.2.1.1 of the datasheet). But TXB outputs provide only 20 µA.
Furthermore, TXB outputs cannot handle a capacitive load of more than 70 pF. This device might not work when you are using cables/connectors.
With the TXB at the output of "System 2", no other bidirectional level shifter is possible. Are the signals really bidirectional?
Thanks for the reply, but I have to ask again, it is also not possible to connect the LSF0101 to the TXB0101? If I see it correctly, the LSF0101 has a low input capacitance and a high output current, right?
Alternatively, what would be a suitable level translator with directional control (the dir pin should then be controlled by the system controller 1 at 1V8) that could be connected to the TXB0101?
The LSF is a passive switch with a drive strength of zero. It outputs open-drain signals; those do not work with the TXB.
A suitable direction-controlled level shifter would be the SN74AXC1T45.