This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: Level Shifter Selection

Part Number: TXB0104

Hello, we'd like to know if below application is suited with TXB010x?

Customer would like to communicate signals between the FPGA GPIO(Biasing power with 5V/3.3V/2.5V) and Gate Driver RDYC pin (Open Drain external pull high 10K Ohm). Since the RDYC pin is dual function pin and it can be bidirectional communication. What we would like to know are:

1. Which of the level shifter is better choice? TXB, TXS and LSF family. Why?

2. What're the major difference between TXB, TXS and LSF family?

3. Which one is good for QSPI, UART communication?