Part Number: SN74LVC2G14
hi,
We only used the channel group of 1A/1Y on Dual Schmitt-Trigger Inverter . As DS requires that unused PIN is not recommended to be suspended, I briefly read the report and only said that it would affect the level abnormality of the corresponding channel.
Please help me confirm the following two questions:
- Whether the suspended channel will affect the used channel, I understand that they are independent of each other
- If the use channel and power supply are not affected, can we suspend the PCB without input and output

thanks.
zhizhao