Part Number: SN74LVC8T245
Other Parts Discussed in Thread: SN74LXC8T245
Hi,
Can I have pull up resistors at the output of the level translator, so that the output is at a defined state when the input is floating
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC8T245
Other Parts Discussed in Thread: SN74LXC8T245
Hi,
Can I have pull up resistors at the output of the level translator, so that the output is at a defined state when the input is floating
Hi Akash,
Can I also suggest the SN74LXC8T245? It has built in dynamic pull-downs if you are worried about floating inputs while switching direction.
The dynamic pull-downs will only activate if the device is disabled in someway and then hold the input low. If you are going to have floating inputs during operation then you will need external pull-ups or pull-downs.
Regards,
Karan