Dear Team,
our customer wants to use CD4047B to design inverter as below.
Spec: Vin :54Vdc Vout:24Vac Watt:50-60W

Is it possible to design like this? Thank you!
BR,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
The maximum input voltage for the CD4047B is 18V. I would not recommend exceeding that, as it could immediately and permanently damage the device.
Also, the outputs probably won't drive enough current to replace a gate driver. I would recommend using an actual gate driver between the CD4047B and the driver MOSFETs.