This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ALVC245: About I / O pin overshoot

Part Number: SN74ALVC245


Hello,

The following URL shows the actual value of the input overshoot of Standard Logic Device.
The Input voltage range (I / O ports) of ABSOLUTE MAXIMUM RATINGS in the SN74ALVC245 data sheet is VCC + 0.5V (max).
Which of the following two is applied to the ability value in this case?
Or is it something other than the following?

1.  Up to about VCC + 1.0V within the period of 10ns
2.  Up to about 1.1 times the absolute maximum rated VI MAX value

https://e2e.ti.com/support/archive/jp/f/analog-read-only/486703/logic-standard-logic-device

best regard,

Goto

  • ALVC inputs do not have a positive clamping diode.

    The only guaranteed limit is that in the datasheet. Please note footnote (1): "Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability." Any larger voltage will degrade the device faster.