Part Number: TXB0104-Q1
Other Parts Discussed in Thread: LSF0108-Q1, SN74AXC4T245-Q1, SN74AXC4T774-Q1, SN74AXC4T774, SN74AXC4T245
Hi team,


Thank you very much for your help.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0104-Q1
Other Parts Discussed in Thread: LSF0108-Q1, SN74AXC4T245-Q1, SN74AXC4T774-Q1, SN74AXC4T774, SN74AXC4T245
Hi team,


Thank you very much for your help.
Best regards,
55 Mbps corresponds to 27.5 MHz.
An auto-bidirectional translator like the TXB (or TXS) cannot do buffering and has weak outputs. All your I²S signals are unidirectional, so you should use a direction-controlled translator like the SN74AXC4T774-Q1 or SN74AXC4T245-Q1. [edited]
hi,Clemens Ladisch
thanks for your help. can we use bidirectional level shifter LSF0108-Q1 because we also have other application, we want to decrease the part category. and the SN74AXC4T774 or SN74AXC4T245 both are not automative part, we should use automative part.
The LSF works at these frequencies only with extremely strong pull-up resistors, which wastes lots of power, and requires the other devices to have high drive strength to avoid too-high low logic levels. You really should use the SN74AXC4T774-Q1 or SN74AXC4T245-Q1.