Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G00DCKR.
Please refer to the below image.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G00DCKR.
Please refer to the below image.
Hi Anusha,
This information is in the datasheet in the Package Option Addendum:
To save you some time -- it's always 260C for standard logic devices.
The time at max is the value you highlighted -- 30 seconds max, which is provided in the image you showed.