This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV123A: max propagation delay

Part Number: SN74LV123A


Hi,

How long is the maximum propagation delay when using 3.3V supply?

The values at 5V supply are described in P12, 9.3 Feature Description of the data sheet.

”The propagation delay has a maximum of 11 ns at 5-V supply.”

Best Regards,

Nishie