This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G06: SN74LVC2G06DCKR Same Marking code but different die

Part Number: SN74LVC2G06


We would want to know why this part has two die sizes?
Another thing is, is all parameter identical to the two die parts?
Does TI have any PCN document to explain that?

  • Hello,

    It is possible that multiple die and package bill of materials can ship against the same material. Die may also be updated or redesigned throughout the lifetime of a material, and a PCN notice would be sent in the case of a change for those who previously ordered the device.

    The topside markings with these two devices (CTJ and CT5) are both valid as per the datasheet package option addendum.

    Any part that we ship will meet the parametric specifications listed in the datasheet:

    https://www.ti.com/lit/ds/symlink/sn74lvc2g06.pdf 

    Best,
    Michael