Other Parts Discussed in Thread: TXU0104, TXU0204, TXU0304, TXB0104, TXB0104-Q1, TXS0102, TXS0104E, SN74LXC2T45, SN74AUP3G34, SN74LVC3G34, SN74AXC4T774-Q1, SN74AXC4T245-Q1, SN74AXC4T774, SN74AXCH4T245, SN74LV4T125, SN74AVC4T245-Q1, SN74AVCH4T245-EP, SN74AVC4T774, SN74AXC4T245, SN74AVC4T245, SN74AVCH4T245, LMK1C1104, SN74AUC125, SN74AUC126, SN74LVC125A, SN74LVC126A, SN74AUP3G17
Hi there, we are looking for a 2-4 bit level shifter from TI to shift between 1V8/3V3 to 5V0. SPI_CLK and SPI_MOSI will be routed through this driver and will go to a relatively long LED strip. The intention is to run the interface at 4 MHz.
We are looking at the following devices for this application:
TXU0104
TXU0204
TXU0304
TXB0104 / TXB0104-Q1
TXS0102
TXS0104E
We have the following questions:
- are any of the devices above not recommended for this application? ie. drive strength, speed
- what is the major difference between the TXB and TXU line? We are familiar with the TSX and TXB drivers.
- besides the different number of bits, how are TXS0102 and TXS0104E different? What does the E represent?
Thanks in advance