Part Number: SN74LVC3G17
Other Parts Discussed in Thread: SN74AHCT125, SN74LXC2T45, SN74LXC1T45, SN74LV1T34
Is SN74LVC3G17 able to do the below two scenario for level shifter application in MD sector?
VCC=5V, Input High Level=3.3V (I think this should be ok)
VCC=3,3V, Input High Level=5V (I'm not sure if this is ok or not?)
Regards
Brian