I need to convert a 2.5 volt logic signal to 3.3 volts to drive M-LVDS drivers.
I would like to use the SN74LVC8T245DGVR with the VCCA=2.5 and VCCB=3.3.
Some of the signals will be Clocks running at about 65 Mhz 50% duty cycle.
Is this the best device to use or do you have a faster device hopefully in the same package?
Also, how noise / jitter would I expect to see in the clocks signals due timing characteristics of the SN74LVC8T245?